Other Parts Discussed in Thread: TPS745-Q1
Hi team,
Could you advise the dropout voltage of TPS785-Q1(VSON package) at 500mA?
Here is my condition :
VIN=1.8V
Vout=1.2V
Iout=0.5A max
Electrical characteristic table's condition is VIN=Vout(nom)+0.75V or 2.0V, and dropout at Vout=1.2V @1A is 800mV.
So I think TPS745-Q1 might be better to consider.
Could you advise?
regards,