Other Parts Discussed in Thread: TPS745
Hi team,
2uF is used for the output capacitor of LP5912.
However, 10 ADCs are connected to the load and 10uF is used for the bypass capacitor of each ADC.
The total amount of capacitors on the output side is 102uF.
Is it necessary to keep it within the maximum capacity of 10uF including the bypass capacitor on the load side?
Best Regards,