Need logic level, VIHmin,VIHmax, VOHmin, VOHmax, VILmin, VILmax, VOLmin, VOLmax, IIHmin, IIHmax, IILmin, IIHmax, IOHmin, IOHmax, IOLmin, IOLmax values. Kindly reply at the earliest
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Need logic level, VIHmin,VIHmax, VOHmin, VOHmax, VILmin, VILmax, VOLmin, VOLmax, IIHmin, IIHmax, IILmin, IIHmax, IOHmin, IOHmax, IOLmin, IOLmax values. Kindly reply at the earliest
Hi Lakshmi
It generates analog voltage. Consider it as constant voltage for reference of your data converter.
Input voltage should be between 11.4V to 36V. It's output will vary from 9.995 to 10.005 V at room temperature and it has 5ppm /C temperature variation. It can provide 10mA max current.
Regards
Trailokya