Hi Expert,
Our customer would like to use MCG53N06AHE3(DFN3333) for LM747000-Q1 application. The work condition is as below. Please help to check if this N MOSFET is applicable or not. Thanks.
BR,
Elec Cheng
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert,
Our customer would like to use MCG53N06AHE3(DFN3333) for LM747000-Q1 application. The work condition is as below. Please help to check if this N MOSFET is applicable or not. Thanks.
BR,
Elec Cheng
Hi Elec,
The Mosfet selected looks good in terms of VDS rating, VGS rating, Gate-Threshold Voltage. The only other parameter we need to consider is the RDS(ON) of the Mosfet - which is 8.2 mohms (max). The acceptable value of this parameter depends on multiple points such as,