Other Parts Discussed in Thread: GPCCHEM
Hello to TI support team ,
I use bq20z655-r1 with 4S3P configuration ICR-18650-26JM Cells chem ID : -2776
I made Golden pack according sequence following recommendation of TI . I received max error =1 . The problem I have is RSOC register mismach at new cells state , I mean i receive the cells from the vendor at voltage 3590mV - 3596mV it set RSOC at start ( 37% - 44% ) in realty if i discharge the battery from this state it has only ~23% of design capacity . After battery fully charged it set 100% and has proper RSOC indicatuin during all discharge period .
How can i repair initial RSOC shift from ~40 % to ~25 % ?
B.R
Alexander Burtakov