Hi all
My customer is working on a design with the BQ25302 and they have this question:
How do the TS and the REGN pins behave when USB is not connected ?
Are they tristate ? What is the internal circuit one has to consider ?
They want to monitor the battery temperature with the uC and at the same time the NTC is connected to the TS pin.
The reference voltage for the NTC is generated by the REGN pin of the BQ25302. If the battery is charged from the USB this works fine.
If the battery is discharged and there is no USB cable connected the REGN voltage is no longer there and they cannot read out the NTC.
Their idea is to put a high level at the ADC2_NTC_REF pin of the uC and to then read out the NTC_OF_Battery pin with the ADC of the uC.
They will do this only if no USB cable is connected. As soon as a USB cable is connected the ADC2_NTC_REF pin will be reconfigured and has again the ADC reference function.
Please also look at the schematic copied below and comment if this works as expected.
Best regards
Ueli