Other Parts Discussed in Thread: UCC2800, UCC2802, UCC2804
UCC2801
Ct=220pF
Rt=36.5k
I am expecting an output frequency between 75kHz and 87 kHz, but I am getting 91.88 kHz. Confirmed in time domain and via FFT.
However, in our hardware implementation, it does work within our range.
This seems to be a fidelity issue with the model; I am using the unencrypted SPICE model provided in LTSpice.
I have also tried the circuit in SIMetrix and the same result
Additionally, it seems like there is no RC design equation in the datasheet for the 2801 model.