Hi Expert,
I see in LP5912-Q1 datasheet that "This device is available with fixed output voltages from 0.8 V to 5.5 V in 25-mV steps.". Does it mean that LP5912-Q1 has 0.8V, 0.825V, 0.05V......5.45V, 5.475V and 5.5V output voltage version? Our customer would like to use LP5912-Q1 to output 0.95V. Is it appliable? If YEs, what's the OPN? Thanks a lot for your help!
BR,
Elec Cheng