This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV707: Inrush current spike at boot-up phase

Part Number: TLV707

Hello support team,

This is FAE Dave, thanks for taking time looking into this issue.

Figure.1 is the limit listed in datasheet and it states that the limit is 450mA of the maximum.

Fig.1

My customer has experienced the current spike during the boot-up, as the figure.2 and figure.3 below.

Fig.2 and Fig.3

Output VR MLCC

1uF*1

Output Device MLCC

22uF*4+47uF*2+0.1uF*2

IIN(fig.2)

1.05A

Pd (instant)

(3.3-1.8V)*1.05A=1.575W

 

Output VR MLCC

1uF*1

Output Device MLCC

22uF*1+0.1uF*2

IIN(fig.3)

932mA

Pd (instant)

(3.3-1.8V)*0.932A=1.398W

My customer has provided me the schematic, if it is needed, I could sent it through email.

Thanks for the support!

Best regards,

Dave