Hi support team,
In the "SUPPLY VOLTAGE AND CURRENT" item of SBVS256A, there is a description that the minimum input voltage value is "Vout + 0.5V".
This value is the value when Iout = 450mA, and when using it at Iout = 100mA, is there any problem with the minimum input voltage value "Vout + 0.1V typ."?
Actually, we are considering using it with the following values.
・ Vin: 5.2V "Designed with double the dropout voltage 100mV typ. (Iout = 100mA) described in SBVS256A."
・ Vout: 5V
・ Iout: 100mA
Regards,
Dice-K