Other Parts Discussed in Thread: SN74AHC1G86-Q1
Hi Team,
In the other E2E thread, a customer synchronized two LM5045 using an external oscillator and a comparator. Our customer would like to synchronize two LM5045 without microcontroller. According to our customer,
We use two LM5045 in our design for more power possibility. We want to synchronize the IC's without using a microcontroller. How is this possible? We tried this by connecting the Rt pin of one controller to the other through the 100pF capacitor. One controller runs at 250kHz, the other one runs at 150kHz. We want to sync them both to 250 kHz without any microcontroller.
Is this solution possible or using an external oscillator is the only solution aside from a microcontroller?
Regards,
Danilo