Hello,
I would like to know if I can wire 2 channels of the TPS2HB35B together in order to get it usuable for a H4 light bulb what have a power consumption of about 60 Watt. I have seen in the datasheet, that the maximum resistor programmable current is about 48 Ampere, what is still a bit too low for the cold resistor values of a H4 light bulb. I know it from other double high side switches that the maximum current is about 30 % higher when I wire it parallel. Is it possible with the TPS2HB35 as well?
Do I need 2 current limiting resistors for it if it is possible or can I use just one resistor if I bridge the current resistor inputs?
Thanks a lot in advance!
All the best!
Axel Joost