When using the miller clamp function of UCC21736-Q1,whether an external MOSFET is needed,or I can refer to this figure directly
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When using the miller clamp function of UCC21736-Q1,whether an external MOSFET is needed,or I can refer to this figure directly
Hi Jiawei,
UCC21736-Q1 features an external miller clamp, and an external MOSFET is needed. Please refer to Figure 50 of the datasheet; it shows how the CLMPE pin should be set up.
Thanks,
Vivian