This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'll try my best to explain what I'm seeing and hopefully, someone can give ideas on what should be looked at.
While the channel is powered up, voltage readings are not really consistent: From 10 readings, at least 1 reading will always output lower value voltage by 10% or even 100%. Meaning, that if TPS works at ~56.5V, the readings go to 36V or even 0V once every few i2c reads. More rarely, even POWER_STATUS (10h) register will flip the bit as "down" or "0" while there were no voltage drops or issues. Note, the I2C transaction is ACKed.
I2C master is STM32F030 configured with "0x00901850" as timing. I've tried setting I2c at a different speed, but it does not seem to affect the issue (ofc, it affects how many times you can read a register in one second) but overall, the issue stays the same.
I'm seeing this with stm32 configured in i2c sync mode and i2c irq mode with no other interrupts running, thus, my estimate is that this should be related to i2c configuration/timing, the board/pcb design, or TPS itself.
Any suggestions will be appreciated.
Just found this topic: https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1087528/tps23881-channel-power-measurement?tisearch=e2e-sitesearch&keymatch=tps23881# and the description sounds familiar.
But my profile has no access to the resources. Is it possible to receive the latest TPS 23881 firmware binary and see if the issue is resolved?
Reinis,
Please go to TPS23881 product page and request access to TPS23881 MySecure folder. Thanks.
Best regards,
Penny
Hello,
When I try to press "Request Now" (link https://www.ti.com/securesoftware/docs/autopagepreview.tsp?opnId=24239) it throws me to "My secure resources" page and shows a message: "There Was An Error Processing Your Request".
Best Regards,
Reinis.
Reinis,
We have manually added you to the MySecure folder. Please check. Thanks.
Best regards,
Penny