Hi Team, Just investigating options to max battery life in battery only mode- is it always set by the battery UVLO value versus the DC to DC converter output voltage. If this was the case could the DC to DC converter operate in 100% duty cycle ( as the device with be operating with very low current ie PFM mode. Also can you explain what the min off time spec refers to? as the SYS input I thought was just an input?