Can the TPS7A4701-EP linear regulator be damaged under the following conditions:
- Back-feeding a 3.3 Vdc voltage source at the linear regulator’s output if there is no 5 Vdc input voltage source.
- Back-feeding a 3.3 Vdc voltage source at the linear regulator’s output if the linear regulator is already operational with a 5 Vdc input voltage source.
The linear regulator has been setup with a feedback resistor string at pin 3 to establish an output voltage of 3.3 Vdc.
The other pins 4-6, & 8-12 are left floating.
Also, we inadvertently shorted the output to return (GND). Please confirm that the linear regulator then would not be damaged with its current limit and thermal shutdown kicking in. It’s designed that way as stated in the data sheet.
I also have some concerns regarding the feedback control scheme being affected with the two conditions stated above. Would there have been some stability issues with the above two conditions that may have resulted in an unstable operation which then may have affected the linear regulator?