Hi Experts,
From the data sheet, I have a question about "Parallel resistor R(P) is recommended to consume 1/2 of the total current at maximum supply voltage.".
I wonder why the Rp is needed?
The Rp connect the In pin and Out pin.
I simulated this device with Rp (100 ohm). And also without Rp.
Please see the result.
Vsupply = 12V, I(Led) = 100mA, Vpwm = 12V & 1000Hz
- Without Rp. The output current I(D2) have no current when V(pwm) = 0
Frist graph is PWM signal. Fourth graph is I(D2)
- With Rp. The output current I(D2) have 50mA current when V(pwm) = 0
So, I wonder why the Rp is needed?
I think 100mA on-off PWM signal is enough to light the LED.