This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8866-Q1: LP8866-Q1 discussion

Part Number: LP8866-Q1

Hi Team

請幫忙釐清下方問題THX

  1. LP8866系列一上電後,如果出現當機現象,無法單存靠I2C指令進行回復,只能透過斷電重啟
  2. LP8866系列,若不進行斷電,則需斷開低壓3.3V端的電,重新上電才能夠重置
  3. 但如果斷開LP8866的低壓端的電源,但其他IO並未進行斷電,如fault/EN/I2C/或有pull Hi的端點有持續供電3.3V,則此種斷電是無效,因為會產生電壓回灌現象
  4. 就認知 Fault腳  應該是開集極的架構,狀態是屬於隔離的,應該不會影響到8866的內部core電壓
  • Hi, Kygo, 

    关于Fault后的动作,可以参见 Table 7-9. Fault and Protection Schemes; 宕机原因是社么? 

    关于电源给电, 可以参见 Figure 7-20. Start-Up Sequence Diagram.  另外, Latch Fault需要拉低ENABLE使退出状态; 

    Regards, 

    Xiaoguang