This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5156-Q1: WEBENCH Power Designer vs LM5155/56 DC/DC Boost Controller Design Tool which one should be used?

Part Number: LM5156-Q1
Other Parts Discussed in Thread: LM5156EVM-BST, LM5155, LM5156

I need a design using LM5156 in boost CCM or DCM mode for input voltage of 12V to 24V and an output voltage variable between 50V to 200V and a current of 5ma max at 200V. I have tried various ways to get the parameters using the WEBENCH Power Designer online version and the LM5155/56 DC/DC BOOST Controller Design Tool (excel version) and using the same input parameters and frequency the results are drastically different in the compensation component values. Which one should be used? How can I get a stable design using the LM5156 chip? I have the LM5156EVM-BST and my own PC board that I have laid out. I can reproduce the 3.5Vin to 12V 3A output design with the same values as in the evaluation board. But I am not able to get the right component values for our requirement of 24Vin to 200V 5ma output design. I can use either CCM or DCM. 

Please help.

Thanks