Other Parts Discussed in Thread: LM5026
Dear TI,
I'm designing a 66-144 VDC to 24 VDC (300W) converter using LM5026 with ACF topology. Regarding SR I have to use conditioning circuit for self-driving of FETs due to secondary high voltage. I have some concern about low-load or no-load DCM operation and its efficiency. Do you think using SR controller ICs (e.g. UCC24610) with SYNC pin employed, alleviate my concerns with significant amount maintaining the robustness considering the peripheral circuit complexity and component quantity compared to conditioning circuit? Does it worth it? And of course I'm open to other suggestions. Thank you in advance.
Best,
Suheyl