Hello Team,
my customer has following question:
The B-version is specified with much higher current limit but has same Rdson as A-version. Also calculation for current limit is different.
But for current sense ratio there is only one value available?
For this application we need to detect 8 Amp. For 8Amp this means we need factor 1500 at SNS output with 5.33mA.
For 5V range it is necessary to use a 820 Ohm sense resistor.
But in a failure case SNS output is driving 4.5mA. Means this that we can measure only with a SNS output range up to 4.5mA which reduces the complete operating current range?
With an 820 Ohm sense resistor this means that a current of 6.75Amp is equal to Fault State.
Is this true and how can we get the full 8 Ampere range for the TPS1HB50B version?
Many Thanks
Josef