Hello,
I am using the TPS7H2201-SP component and I am unable to switch off the load. I have a 5V input, when I turn the enable low my output only reduces to 1.3V
This is my implementation. The enable signal has no noise. I measured some of the other pins when EN = 0V
CS: 0.1V
OVP: 0.49V
RTIMER: 0V
IL: 0.113V
ILTIMER: 0V
SS: 5V
VOUT: 1.3V
The device turns on as expected.