Hi,
Need to design Constant current mode buck converter, Could any one suggest control IC for the same.
Unable to use LM3495 as need to use external switch as voltage rating for input and output bit higher side.
Input:300V to 400V Dc
Output 0-50V DC 10A or 12 A Constant current.
Reg,
Harsh