I used Webench to Design a DC to DC converter. The input voltage is 3.3+/- 10% with an output of 6V. It is to drive an adjustable constant current source in the range from 10mA to 30mA, so I chose a 0.5A DC to DC design to give ample headroom. When I load the DC to DC converter with about 25mA, the 6V output voltage starts to drop. Any suggestions?
Here's a link to the design. https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=4CB53CBD8F8ECD0B