Other Parts Discussed in Thread: TEST2
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Tino,
scanning thru the datasheet, it look to me the VFV Ripple is the expect ripple at the FB that corespend the VOUT.
For example for ripple of 30mV ripple and with VO=1.8V, R2=10K, i can calculate R1=13K
Tomoya is traveling today, he can provide more inputs later on
Thanks!
Tahar
Hi Tino,
The VFB1(ripple) in the datasheet corresponds to the VOUT ripple divided down by the ratio of the feedback resistors plus the internal ripple injection voltage. The RC time constant of the internal ripple injection circuit is 175us for 350kHz operation and 88us for 700kHz operation. To calculate the internal ripple injection voltage, replace L1 in Equation 4 from the datasheet with the RC time constant. To calculate VOUT ripple, solve Equation 10 in the datasheet for Vo1(ripple), where C1 is the output capacitance. To reflect VOUT ripple to FB pin, multiply VOUT ripple by VREF divided by VOUT. VREF=0.765 if TEST2=GND and VREF=0.758 if TEST2=V5FILT.