This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14010A: LMR14010A Vin disconnection trouble

Part Number: LMR14010A
Other Parts Discussed in Thread: LMR54410, LM5158

Hi all,

I've been testing LMR14010AEVM Evaluation board and I have a trouble. I've modified PCB for VIN=35V, Vout=27V/750mA, Cout = 4.7uF x2 + 100nF

With Resistive Load is working out up to 750mA , but DC-DC has broken when I disconnect and connect  VIN positive wire with a Switch and maximum load, the VIN power is a PSU Lab with Current limit 1A.

I've made the test with the same PCB and LMR54410 PN(So the Vout = 28V/800mA ) and the effect was the same, IC was broken as well.

Thanks in advance.

Juan Carlos