I've attempted to simulate the TPS5430 reference design, but have been unable to do so. The output should be around 5V, but the simulation result gives a few mV. I am simulating the circuit because I want to make some changes to the reference design, but I need to get the simulation of the reference design working first.
The reference design is shown below directly from the datasheet. I am using pspice for TI to simulate the circuit because I thought it had the highest probability of success.
I apologize if this was posted in the wrong forum. I also apologize if I have missed something. I am new to pspice for TI and this is my first time using this IC.