Hi Ti Team,
The BQ25611D currently used by the product has entered the PV Stage. The following problems have been confirmed during the test: 1) At present, when Min System voltage is set at 3.5V and the battery is not connected, the System cannot be started normally. After the Min System voltage is changed to 2.8V, the System can be successfully started without battery connection. In the figure below, Dc to Dc boosts/depresses to 3.8V for System use. I want to know why the change of Min System voltage, except Vsys from 3.68V to 2.98V, will there be any other impact on the function of Charger?