Other Parts Discussed in Thread: TLC5948, TLC59283, TLC5929
Hello guys,
One of my customers is evaluating TLC5948A for just LED on/off control because they don't need PWM dimming for their next products.
Their controller is poor. So they can use three GPIO ports only and they can not supply GSCLK signal separately.
At this moment, they control SIN and SCLK by two GPIO ports. They tie LAT and GSCLK together and control those signal by remaining one port.
They control LED turn on/off by BLANK bit of the function control latch data bit 119.
For LED turning on, they wrote non zero data to GS data latch at first. After that, they wrote "0" to BLANK bit. Then LED was turned on.
For LED turning off, they wrote "1" to BLANK bit. Then LED was turned off.
At this moment, they have the following question. Could you please give me your reply?
Q. This result is good for them.
But is this control method not problem?
Best regards,
Kazuya.
.