Hi,
A medical customer would like a suggestion for a 8-13Vin to -5.7 at 2A(max) inverter.
Do we have such a device to offer? Converter with integrated FETs would be an advantage.
Thanks,
VL
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
A medical customer would like a suggestion for a 8-13Vin to -5.7 at 2A(max) inverter.
Do we have such a device to offer? Converter with integrated FETs would be an advantage.
Thanks,
VL
Hi Victor,
LMZ34002 input voltage range from 4.5 V to 40 V, output voltage range from –3 V to –17 V and output Current is 2A, so it is suitable.
B R
Colin
Thank you Colin,
I have looked at the LMZ34002, however when I try this simulation on the Webench it states that this design can't be created.
Could you please confirm there won't be any issues?
Thanks,
VL
HI Victor,
If output current is no more than 2A(max), this device is OK to meet customer requirements.