Hi,
i am using UC2843A for a low voltage flyback. (20V .. 60V input and 24V output with 2.7A and 200KHz). i choose all the parameters as in Webench design recomendation.
Vref (5V) is constant and OK. RC pin is also OK. CS pin is also OK (i have slop compensation and i can see a fraction of my RC voltage in this pin).
Problem is that with activation of VREF pin, the comp pin is also activated and rises from 500mV to 800mV. it does not reach VOL of error amplifier and won't let IC to generate any PWM signal on the out pin.
How can i correct this? i have a parallel 1nF and 10KOhm between comp and feedback with 5KOhm between feedback and secondary side opto. i also tried different resistor combination. this resistor should be able to sink the error amplifier current and there is a minimum value for it. 10KOhm should be OK. what is the startup process of Comp pin?
Thanks in advance