Table 7.1 Absolute Maximum Ratings in the data sheet SLVSF07A specifies that the maximum voltage is 3.3V, yet the PSPICE simulation provided in slvmdq0.zip produces a peak voltage of 5V at the COMP pin shortly after the output voltage is shorted in the simulation. Is that realistic?
What is the highest voltage that the COMP pin can deliver due to the error amplifier? Also what is the minimum output voltage from the error amplifier at the COMP pin?
Also, the provided PSpice model is very slow. It takes several hours to run on a fast computer with 8 Xeon cores and 256 GB of RAM. This is with the latestFlyback Simulation.pdf version of PSpice A/D 17.4.