Dears
We have an application of DCDC with 15V input and 5V output, in this case, the UCC27211 have 12V supply to drive the MOSFET. We have found the high side output not follow the high side input, when the DCDC load current increase.
So we are wondering if there have some internal protection except the UVLO? If the voltage on the Cboot is very stable of 11.7V, is there any possible that this device output not follow the input of the high side driver? the low side works well.
Thanks
Jun Shen