Dear TI support team,
We have facing issue with the PMIC unable to output any power from LDOx_OUT and SMPSx_SW_x even input power is correct.
The product is under production, and found more than 10 pcs of card have the issue.
Hopefully, can get your advice for this case.
Below the measurement is done during debugging.
POWERGOOD = 0V,
REGEN1 = 0V
RESET_IN = 0V, observed a litter bit up in the oscilloscope (0.2V)
RPWRON = 5V
ENABLE1 = 0V
POWERON = 5V
BOOT0 = 0V, observed a litter bit up in the oscilloscope
BOOT1 = 0V, observed a litter bit up in the oscilloscope
VCC SENSE = 5V
VCC SENSE2 = 5V
LDOVRTC_OUT = 0V, observed a litter bit up in the oscilloscope (0.2V)
Thank you.
Regards,
Chee Hong