This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25700A: Charging LiFePO4 1S battery using PMIC

Part Number: BQ25700A

Hi TI,

As per the datasheets the Max charge voltage for 1S configuration is 4.192 mV . 

But  the Battery I'm using  is LiFePO4 1s 3.2V 2200mAh,  The Max charge  voltage for this Battery is 3.6V .

so my Question is

1) can BQ25700A  Automatically changes  the Maxcharge voltage to 3.6V for LiFePO4 battery  ? or it will charge the Battery to 4.192mV  which is Default for 1S configuration 

2) After Every POR the default value for Maxcharge voltage register is 4.192mV  so if it cannot detect LiFePO4 battery 3.2V then every time i need to Program the registers manually ?