I am component engineer working with Honeywell Aerospace. Can you please share Operating temperature Range for TI MPN ‘LP395Z/LFT1’ since it is not specified in the datasheet.8446.Doc1.docx
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am component engineer working with Honeywell Aerospace. Can you please share Operating temperature Range for TI MPN ‘LP395Z/LFT1’ since it is not specified in the datasheet.8446.Doc1.docx
Hi Team, Any Update?
We need information on priority!
Hi Rashi,
Apologies for the delay.
The LP395/LFT1 is rated for operation over a −40°C to +125°C range.
Both lead options were tested under the same reliability tests.
Best Regards,
Elizabeth
Thanks Elizabeth for the details.
I also wanted to know what is the difference between LP395Z/LFT1 and LP395Z/NOPB? Is the only difference is in lead options? If Yes, what lead option both of these parts have? Since, it is not clarified in the datasheet, please help in answering the same.
Hi Rashi,
Yes, the difference between the OPNs is the lead options. The LP395Z/LFT1 is Formed lead and LP395Z/NOPB is Straight lead.
Best Regards,
Elizabeth