Other Parts Discussed in Thread: TPS25740A, , TPS25750
HI Sir
Due to TPS25740A out of stock, I need to choose another solution
Could you share the different table between A & B?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alex,
The main difference between these two PD controllers is the B variant is USB PD 2.0 certified (TID# 1030004) and USB PD 3.0 Compliant Power while the A variant is only USB PD 2.0 Certified Provider and USB Type-C Rev. 1.2 Compliant Source.
The TPS25740B can advertise 5V/9/V/12V/15V/20V with 8 options for pin-selectable peak power settings ranging from 18W to 100W while the TPS25740A can advertise 5V/9V/15V with 11 options for pin-selectable peak power settings ranging from 15W-81W. Both have very similar high voltage and safety integration, the B variant has 3-pin external power supply control while the A variant only has 2-pin.
Please do note for both variants, it is listed as a NRND (not recommended for new designs) device. If you're looking for more up-to-date PD controllers similar to this model, I would recommend looking at the TPS25750 as we can provide more support for it.
Regards,
Raymond Lin