This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear,
our client use UCC28780 and UCC24612 and TPS25740B for 65W Type-C Application
Could help me suggestion schematic and layout as below file.
schematic:
Transformer design information:
Lm= 65uH ,Lk=2uH
turn ratio => Np:Ns:Naux1:Naux2:Nas=28:4:4:9:4
layout::
BU651.011A1+BU651.012A1+BU651.013A1.pcb
If any question, Please advise me.
Thanks,
Best regards,
Lawrence.