This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53515: set OCP to 14A

Part Number: TPS53515
Other Parts Discussed in Thread: TPS3514

Hi

in #7.3.6 Current Sense and Overcurrent Protection

it show "For the TPS53515 device, the overcurrent protection maximum is recommended up to 14 A only. "

but in webench @ power design, I only can set 12A.

what " Rtip vaule ""I can use , for 14A.

or TPS3514 itself have 14 OCP ?