This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3410-Q1: SEPIC Operation below 3.0V

Part Number: LM3410-Q1

Hi team,

I would like to use LM3410-Q1 as SEPIC topology.

Input is 3.3V regulated supply and output LED is 2.6V to 3.3V Vf.

LM3410-Q1 recommended operating output range is specified as >3V. 

In my condition, is that possible to regulate the output below 3V? 

Please advise if there is any concern.

regards,