Other Parts Discussed in Thread: TPS3808
Hi,
I am using the TPS3838 as an open-drain voltage supervisor for a Bluetooth module's VCC.
I also have the push-pull output 'PROG_RSTn' from a TLC555QDRQ1 connected to the same node. There is a possibility where PROG_RSTn drives high and RESETn open-drain pin drives low and that would short 3.3V to GND. I want to change R14 from 0 ohms to a value that would limit the current if this situation were to arise. Do you know what is the max operating sink current that the RESETn pin can handle?