This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A8300: Layout rules of Pin2 SNS

Part Number: TPS7A8300

Hi Sir,

Pls confirm layout rules of Pin2 SNS, such as the width of routing. If there is a 0R resistor bewteen SNS and Output, should we place the 0R to Sink side or Source side?

  • Hello,

    The routing can be minimum size because it is not a current-carrying trace. 

    I don't understand your question about the 0R. What do you mean by sink side or source side? Are you saying at the "top" of the load, i.e. where VOUT is regulated, or the "bottom" of the load, where the load current flows out of the load?

    Thanks,

    Nick

  • Hi sir,

    Sink side ,is the load side, where the load courrent flows to the load. The Remote sense.

    Source side, where Vout decouple Cap side. The Near end sense.

  • Hello,

    The SNS trace should connect to where the load is at. The output capacitor should still be close to the LDO, and the SNS pin should be connected to where the load is delivered.

    Regards,

    Nick