Other Parts Discussed in Thread: BQ25616,
This is the charging status waveform
This is the first case :-
Bat voltage:- 3.65v
when we connect the battery and as you see the mark in graph wave goes to low. and charging status low.
Note:- after mark waveform goes to low because I try to out the battery from connector and again connect the battery.
This is the proper working!!
This is the Second case :-
Bat voltage:- 4.105v
In this case when we connect the battery you see in graph the mark wave not going to low. its just try to low but they just come to high and charging status stuck at High.
Note:- after mark waveform goes to low because I try to out the battery from connector and again connect the battery. But RESULT is same.
This is the issue in charging ic!!
This problem occurs in only Battery range of voltage 4.01v to 4.19v.
PLEASE HELP ME IN THIS CASE.
THANK YOU!!