Hi,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
what is the data rate from processor though AUX channel?
Hi,
Are you referring to the 0.28V seen on AUXP/AUXN? If you look at the DP AUX bus block diagram as shown below,
that common mode voltage is determined by the source (TX) itself.
Thanks
David
Hi David,
Any idea why the DC bias at pin27 (SBU1) and pin24 (AUXP) is only 0.062Vdc since I am using a 100kohm resistor? Thanks.
Hi,
On AUXP, you have a 100k strong pulldown. There should be a weak pullup to 3.3V (typical 1M). In the example of a strong 100k pulldown and weak 1M pullup, you will see ~0.3V. So 0.062V is a possible voltage depending on the weak pullup resistance on the sink side.
If you look at the common mode voltage requirement in the TUSB546 datasheet, you can 0.062V is within the spec.
Are you connecting to a Type-C monitor? If this is the case, do you have a PD controller that controls the TUSB546?
Thanks
David
Hi David,
Yes. I am connecting to a Type-C monitor. The TSUB546 is set to GPIO mode. The PD controller only controls the FLIP logic to the TSUB546.
I also tried connecting the TSUB546EVM to the Type-C monitor and is able to get 0.3Vdc bias at SBU1/AUXP pin. Does setting the USB-C port to DFP or UFP by the PD controller affects the DC biasing of the SBU channel from the monitor? Thanks.
Hi,
I would recommend letting the PD controller controls the TUSB546 CTL0 and CTL1 as the PD controller may set the TUSB546 into 2DP or 4 DP lanes depending on the PD controller CC negotiation with the Type-C monitor.
Does setting the USB-C port to DFP or UFP by the PD controller affects the DC biasing of the SBU channel from the monitor?
No, the DC bias is only controlled by the external pullup/pulldown on the AUX bus, when the TUSB546 is being configured into the DP mode.
Thanks
David