This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79652-Q1: Set All pins as Thermistor Input

Part Number: BQ79652-Q1
Other Parts Discussed in Thread: BQSTUDIO

Hello 

 

We are trying to use CFETOFF pin to sense the temperature. In order to do so we are using an external NTC with a 18kohm internal pullup resistor as raw value count.

Command Sequence is as follows:
W: 10 3e 90 00 - start config
W: 10 3e fa 92 3b - CFETOFF config
W: 10 60 38 05 - checksum
W: 10 3e 92 00 - End config
R: 10 6a 2 - without ground -data:- AC 4C
R: 10 6a 2 - when grounded -data:- 20 02


Could you help us in understanding the meaning of above values ?

We even want to set all pins with same configuration.

Regards 

Nisha