This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54140A: Can't simulate at 2MHz

Part Number: TPS54140A


Hello,

I'm having trouble reaching my desired simulation frequency on Webench.

I am trying to buck 16V to 6V @1A, however the switching frequency is capped at 1.321 MHz..

What could be limiting that switching frequency and how can I increase it?

Thanks,

Snir

  • Hi Snir,

    Thanks for bringing awareness to this issue. I believe this is due to an issue with the data provided to the Webench team, but I will check on that. Can you check a simulation with the TINA/PSPICE model and see if you have any issues there?

    Regards,

    Richard