Hi Team,
Can you help me confirm the best way to put an LGPO into Tri-State?
1. The first method I'd expect would be setting the LGPO as a command controlled GPO in Hi-Z and seems to be the most simple.
2. The second method looks to be adding the pin, configuring to Active High, Open-Drain, and being able to set a delay with no logic: Ie Delay = 10ms * <No Logic>
My understanding is this would hold the pin low for 10ms on power up and set to Tri-State afterwards, correct?
3. The third method could be deleting the LGPO from configuration and leaving unassigned.
What behavior might I expect from leaving the LGPO unassigned?
The LGPO in question this time is D5, but would expect applicable to all LGPO.
Best Regards,
Jacob Butler