Using the CHEM ID matching tool. It looks like we have an good ChemID match for our battery, but is it okay that the capacity is different? Our battery is a 2000mAh cell and the recommended ID is for a 10000mAh cell?
Best chemical ID : 256 Best chemical ID max. deviation, % : 2.88
Summary of all IDs with max. DOD deviation below 3%
Chem ID max DOD error, % Max R deviation, ratio
256 2.88 0.59
Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge.
Nick Carley