Part Number: TPS61235P
Hi,
Please review my schematic below

The voltage and current will come from a LIPO Battery(3.7V/6000mAh). I'd like to boost converter to output 5.1V and 3A max as my output will be going to my load which will be a Raspberry Pi 4b. I'd like to use the CC feature to limit the current to around 3A for safety reasons. I calculated the worst case input_avg current to be around 5.2427A. Please see if my capacitance values are also fine. I will not be able to pull EN high or low whenever I'd like to so I tied EN to VIN.
Thank you so much,
Andy