This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM43601: Output of -12V not generated with a load of 500mA

Part Number: LM43601

Hi There,

We have made same circuit for -12V as per THIS POST in Ti E2E forums. While doing output voltage ripple measurements at a load of 500mA, we observed that output of -12V is not being generated and there is a current flow of nearly 140mA in the load. This scenario happens when we are connecting load and then powering ON the input supply of +12V.

In case, we power ON the input supply and then connect the 500mA load then everything works fine. Please let me know if there is any solution to overcome this issue other than increasing the input supply voltage.

Thanks..!!!